How can we build i.MX8QM Surround View Application ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can we build i.MX8QM Surround View Application ?

1,691 次查看
mamorukanou
Contributor IV

Hello, community.

I'm trying to run a surround view demo on i.MX8QM-MEK according to i.MX Surround View Application (SVARM Rev.1 07/2018).

https://www.nxp.com/webapp/Download?colCode=SVARM 

The latest 8QM evaluation board (IMX8QM-MEK) seems to have RevB silicon.

******
U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (May 18 2019 - 00:38:39 +0000)

CPU:   Freescale i.MX8QM revB A53 at 1200 MHz at 23C      <--- RevB Silicon
Model: Freescale i.MX8QM MEK

******

This document has kernel version L4.9.51-beta2. In addition, the silicon version of i.MX8QM assumes RevA.

L4.9.51-beta2 's boot-loader does not seen to start with latest i.MX8QM RevB silicon.
There are two possible ways to run on RevB silicon.
1) Build L4.9.51-beta2 BSP  with RevB (need SCFW for RevB ? )
2) Modify the SD3D-1.1 surround view applications to work with L4.14.98 (This version is OK for RevB)


Either way, can anyone tell me the procedure to work with RevB silicon?

Or do you have oter any good ideas?

Best Regards,

Kanou

1 回复

1,472 次查看
joanxie
NXP TechSupport
NXP TechSupport

for revB, suggest that customer can use latest version,one can use 4.14.98, then you can follow the surround view reference manual,

i.MX Surround View System | NXP 

0 项奖励
回复