How can I test JB4.3 “webrtc(web real-time communication)” function in i.MX6Q Sabre SD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I test JB4.3 “webrtc(web real-time communication)” function in i.MX6Q Sabre SD?

ソリューションへジャンプ
8,800件の閲覧回数
yangruihero
NXP Employee
NXP Employee

Dear:

I have found that JB4.3 has added new "webrtc" feature in "i.MX6 android_jb4.3_1.0.0 Android Release Notes", could you please provide some detailed information about this function?

How can I test JB4.3 "webrtc(Web real-time communication)" function in i.MX6Q Sabre-SD?

Thank you very much!

ラベル(2)
1 解決策
7,954件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi,

According to the log, that seems to be related with chromium browser. These is a similar open issue on chromium.

http://code.google.com/p/chromium/issues/detail?id=362348

Regards,

Max

元の投稿で解決策を見る

0 件の賞賛
返信
16 返答(返信)
7,954件の閲覧回数
norisugi
Contributor II

I tested the WebRTC using the Chrome with UVC USB Camera.

Then the browser crash occurred.

It seems that audio driver crash.

I attach the adb log.

Could you check it ?

0 件の賞賛
返信
7,955件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi,

According to the log, that seems to be related with chromium browser. These is a similar open issue on chromium.

http://code.google.com/p/chromium/issues/detail?id=362348

Regards,

Max

0 件の賞賛
返信
7,954件の閲覧回数
norisugi
Contributor II

Currently I can't judge whether this issue is due to the browser or not.

I got the another adb log.

Could you check the attached file ?

0 件の賞賛
返信
7,954件の閲覧回数
max_tsai
NXP Employee
NXP Employee

Your attached log also looks similar as Issue 362348 - chromium - [Android-WebRTC] Crash in accessing WebRTC page with external USB camera -...

--

I/DEBUG   ( 2358): backtrace:

I/DEBUG   ( 2358):     #00  pc 0001e684  /system/lib/libc.so

I/DEBUG   ( 2358):     #01  pc 0001c550  /system/lib/libc.so (abort+4)

I/DEBUG   ( 2358):     #02  pc 000121f1  /system/lib/libc.so

I/DEBUG   ( 2358):     #03  pc 00011701  /system/lib/libc.so (__assert2+20)

I/DEBUG   ( 2358):     #04  pc 01bf1649  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #05  pc 01bf173d  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #06  pc 01bf3c6b  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #07  pc 01aad261  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #08  pc 01a9a74b  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #09  pc 01ab2d9b  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #10  pc 01aab13d  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #11  pc 00b82601  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #12  pc 00b7fe33  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

--

Regards,

Max

0 件の賞賛
返信
7,954件の閲覧回数
norisugi
Contributor II

Thank you for your information.

My issue has been fixed by the workaround of the WebRTC project.

Many thanks !

0 件の賞賛
返信
7,954件の閲覧回数
EricNelson
Senior Contributor II

Hi Nori,

Do you have a reference to the fix?

0 件の賞賛
返信
7,954件の閲覧回数
norisugi
Contributor II
7,954件の閲覧回数
EricNelson
Senior Contributor II

Thanks Nori.

0 件の賞賛
返信
7,954件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

MaxTsai can you continue with the  follow up?

0 件の賞賛
返信
7,954件の閲覧回数
YixingKong
Senior Contributor IV

Rui

Since there is no reply from you, I am closing the DI. If your issue still exists please come here again and reopen the DI.

Thanks,

Yixing

0 件の賞賛
返信
7,954件の閲覧回数
YixingKong
Senior Contributor IV

Rui, are you ok to close the DI?

Thanks,

Yixing

0 件の賞賛
返信
7,954件の閲覧回数
EricNelson
Senior Contributor II

Actually, this doesn't answer the question, it just brings up another:

How do you install Chrome?

(Chrome isn't a part of the stock build)

We've tested WebRTC successfully in the 4.2-beta using the Mozilla Fennec browser

as described here:

     http://boundarydevices.com/second-release-jellybean-4-3-beta-mx6/

0 件の賞賛
返信
7,954件の閲覧回数
max_tsai
NXP Employee
NXP Employee

Sure, you can use firefox browser for Android instead of Chrome. That blog shows how to use Firefox also.

Since Mozilla starts to support webRTC since Firefox 24, you can install lastest Firefox for Android without Aurora.

Then you test by Mozilla gUM test page as you describes in your http://boundarydevices.com/second-release-jellybean-4-3-beta-mx6/

Or you can test by palava.tv

7,954件の閲覧回数
EricNelson
Senior Contributor II

:smileyhappy: And the https://palava.tv/test URL is much easier to type!

0 件の賞賛
返信
7,954件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

MaxTsai please continue with the follow up.

0 件の賞賛
返信