How can I set the uart2 map to sdma2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I set the uart2 map to sdma2

4,648 次查看
hongxingyu1982
Contributor III

Hi sir

Now I used the imx8mq board and I see the uart2 event map to the 24 and 25 channels of sdma1 as blew:

pastedImage_2.png

Can I map the uart2 to the channel of sdma2, if it can, how can I set it ?

Thanks.

0 项奖励
回复
8 回复数

4,575 次查看
hongxingyu1982
Contributor III

Hi igor

How can I test the function of sdma1 in imx8mq board? Could you help to supply the test demo ?

Thanks

BR

0 项奖励
回复

4,575 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hongxing

 

if you have special need for changing default sdma configuration

suggest to apply to :

Commercial Support and Engineering Services | NXP 

 

Best regards
igor

0 项奖励
回复

4,575 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hongxing

>Can I map the uart2 to the channel of sdma2, 

not, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,575 次查看
hongxingyu1982
Contributor III

Hi,igor

Thank you so much for your reply.

Why? could you show me more details?

Br//Hongxing

0 项奖励
回复

4,575 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hongxing

 

one will have to write custom sdma script.

 

Best regards
igor

0 项奖励
回复

4,575 次查看
hongxingyu1982
Contributor III

Hi igor

> one will have to write custom sdma script.

Which scrpit, could you show me a reference ?

Br//Hongxing

0 项奖励
回复

4,575 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hongxing

 

>Which scrpit, could you show me a reference ?

sorry writing custom scripts is not supported by NXP.

So one will have to use existing scripts.

 

Best regards
igor

0 项奖励
回复

4,575 次查看
hongxingyu1982
Contributor III

HI igor

Ok. 

But if I really want to do map the uart2 to the channel of sdma2, how can i do it ? Is there is others ways ?

Br//Hongxing

0 项奖励
回复