How IMX selects SPI at Boot Time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How IMX selects SPI at Boot Time

1,742件の閲覧回数
adityanagal
Contributor III

Hi ,

I am working over IMX6 solo and in my design NOR Flash is interfaced over SPI3. I want to know , during booting time( Internal boot) , how IMX6 will get to know on which SPI NOR flash is present.  IMX6 solo support multiple SPI , so how IMX6 determines the SPI where NOR flash is present. Please suggest.

Regards,

Aditya Nagal

0 件の賞賛
返信
2 返答(返信)

1,660件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Aditya,

You can select the boot option with the eFUSES,  you can review the  (BOOT_CFG4)  which selects the SPI port that it is going to be selected for booting.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,660件の閲覧回数
adityanagal
Contributor III

Thanks a lot!!

Regards,

Aditya Nagal

0 件の賞賛
返信