Host freezes/Hangs while building

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Host freezes/Hangs while building

1,077 Views
purendra1991
NXP Employee
NXP Employee

Hi,

I am building imx-image-full on my host machine for imx8mqevk and it freezes every now and then, I started top command and found out that cpu utilization is 100% sometimes or close to 100% most of the time (attaching the screenshots for reference).

By default bitbake was using 8 tasks/threads, I thought making it 4 ( BB_NUMBER_THREADS = "4" in local.conf ) might be a way because so that all my cores aren't busy.

But even then the situation is same as before, please suggest me what should I do to successfully build my image.

My Host configuration are i5 with 8gb RAM and I am using Ubuntu 20.04 LTS.

LinuxYoctoCrash1.jpg

 

LinuxYoctoCrash2.jpg

 

Labels (1)
0 Kudos
Reply
0 Replies