Hold time control for NAND flash.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hold time control for NAND flash.

1,886件の閲覧回数
takayuki_ishii
Contributor V

Hello community,

I'm trying to configure GPMI NAND I/F timing for i.MX6Dual.

Current GPIM_TIMING0[DATA_HOLD]=3 and GPIM_TIMING0 register value is a  0x00010303.

But write cycle waveform output only 1cycle width.

Other bit value, GPIM_TIMING0[ADDRESS_SETUP] and GPIM_TIMING0[DATA_SETUP], seems correctly.

Do you have some checkpoint to solve this problem?

Best regards,

Ishii.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,816件の閲覧回数
takayuki_ishii
Contributor V

Hello jamesbone‌

Thank you for your reply and sorry my late reply.

This problem occurs by u-boot setting.

NAND device is a Macronix MX30LF4G18AC .

Best regards,

Ishii.

0 件の賞賛
返信

1,816件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

Are you doing the setup for Uboot?  or directly in the DTS,? which NAND memory you are trying to use?

You can check

Linux Guide in Linux Documentation

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

0 件の賞賛
返信