High current consumption of PFuze100 SNVS RTC battery

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

High current consumption of PFuze100 SNVS RTC battery

1,570件の閲覧回数
mayqueen
Contributor IV

Platform: IMX6Q
OS: Android 7.1, BuildRoot201611

This issue is happen after cutting off the power, the RTC battery current consumption is about 200-300mA,

it means the life of coin battery is only 2-3 weeks, it doesn't make sense, but it's a known issue when I search on community...

But our circuit is the same as SABRESD board on PMIC part, it's impossible demo board always exist this issue, so please help us to double confirm it, I think it's not software issue.

Thank you so much
ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,443件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Can you please confirm where you are measuring the RTC battery current consumption, where in the schematic you are opening to measure this current consumption?


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信