Hi-Z_FOR_BOOT_B in SABRE AI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi-Z_FOR_BOOT_B in SABRE AI

ソリューションへジャンプ
2,424件の閲覧回数
jeevanmahadevu
Contributor II

Why  Hi-Z_FOR_BOOT_B is provided during the boot only for Touch interrupt, Magnetometer interrupt, GPS interrupt, UART3_RTS of Bluetooth and for USB_HOST, Not for any other peripherals ?

1 解決策
2,315件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

because these signals are connected to boot configuration

lines, like EIM_EB1(COMPASS_INT) on p.9 SPF-27142

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,315件の閲覧回数
jeevanmahadevu
Contributor II

Thank you very much igor

0 件の賞賛
返信
2,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

because these signals are connected to boot configuration

lines, like EIM_EB1(COMPASS_INT) on p.9 SPF-27142

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------