Hello everyone,
I'm playing with WinCE700 and my BSP is iMX53_QSB and could download image via ethernet (through switch) but Can't transport via KITL if enable KITL it will stuck in OEMInit and can't fetch file system. I've Confused and felt lost
in this problem anyone got the same problem as I do :smileycry: ?
解決済! 解決策の投稿を見る。
Hi Chang
please look at
How to use KITL to debug i.mx53
also look at recommendations of WCE700_MX53_ER_1105_SMD_UserGuide.pdf
IMX53_TABLET_1105_WCE7_BSP_DOCS
-active / passive KITL modes of target i.MX53 (Eboot)
should meet host PC (Platform Builder) configuration.
If the SMD board is configured for active KITL, the image waits for a
Platform Builder connection before booting the OS image. Because the OS
image is already resident in Flash memory, it is necessary to reconfigure the
Platform Builder to jump directly to the image by selecting Target >
Connectivity Options > Core Service Settings > Download Image:
Never (jump to image).
-section 5.3 (Platform Builder Limitations/Issues):
Connection to Platform Builder Remote Tools may fail.
Workaround :
Network configuration for PC workstation may have MTU
(Maximum Transmit Size) size set to less than 1500, which is
not compatible with the KITL MTU size.
Best regards
igor
Hi Chang
please look at
How to use KITL to debug i.mx53
also look at recommendations of WCE700_MX53_ER_1105_SMD_UserGuide.pdf
IMX53_TABLET_1105_WCE7_BSP_DOCS
-active / passive KITL modes of target i.MX53 (Eboot)
should meet host PC (Platform Builder) configuration.
If the SMD board is configured for active KITL, the image waits for a
Platform Builder connection before booting the OS image. Because the OS
image is already resident in Flash memory, it is necessary to reconfigure the
Platform Builder to jump directly to the image by selecting Target >
Connectivity Options > Core Service Settings > Download Image:
Never (jump to image).
-section 5.3 (Platform Builder Limitations/Issues):
Connection to Platform Builder Remote Tools may fail.
Workaround :
Network configuration for PC workstation may have MTU
(Maximum Transmit Size) size set to less than 1500, which is
not compatible with the KITL MTU size.
Best regards
igor
Hello Igor,
Thank you for kindly advice :smileylaugh: ! I've reading your useful information and after change eboot and set KITL work mode as interrupt, enable KITL enable mode and finally success:smileylaugh: !!
But when start remote tool like FileViewer, it end up restart like following :smileycry: anyone encounter the same problem as I do?
Sincerely,
Chang
Hi Chang
probably it is more suitable to post this to microsoft FAQ forum,
like below
USB KITL and USB OTG driver conflict
~igor
Hi igor,
I read your post and change MTU size, but Remote tool still error in message 0xC000005 and I connect device through Ethernet (via switch).
Truly grateful for your sharing and advice, I'll try to post to microsoft FAQ too :smileylaugh:. Wish you have a nice day !
Sincerely,
Chang