Hi, My BSP is iMX53_QSB WinCE700, I could download image via ethernet but Can't transport via KITL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, My BSP is iMX53_QSB WinCE700, I could download image via ethernet but Can't transport via KITL

Jump to solution
1,057 Views
changhsin-wen
Contributor II

Hello everyone,

  I'm playing with WinCE700 and my BSP is iMX53_QSB  and could download image via ethernet (through switch) but Can't transport via KITL if enable KITL it will stuck in OEMInit and can't fetch file system. I've Confused and felt lost

in this problem anyone got the same problem as I do :smileycry: ?


build option.png


conective option.png

boot menu.png

OEMinit.png

Labels (1)
Tags (1)
1 Solution
800 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chang

please look at

How to use KITL to debug i.mx53

also look at recommendations of WCE700_MX53_ER_1105_SMD_UserGuide.pdf

IMX53_TABLET_1105_WCE7_BSP_DOCS

-active / passive KITL modes of target i.MX53 (Eboot)

should meet host PC (Platform Builder) configuration.

If the SMD board is configured for active KITL, the image waits for a

Platform Builder connection before booting the OS image. Because the OS

image is already resident in Flash memory, it is necessary to reconfigure the

Platform Builder to jump directly to the image by selecting Target >

Connectivity Options > Core Service Settings > Download Image:

Never (jump to image).

-section 5.3 (Platform Builder Limitations/Issues):

Connection to Platform Builder Remote Tools may fail.

Workaround :

Network configuration for PC workstation may have MTU

(Maximum Transmit Size) size set to less than 1500, which is

not compatible with the KITL MTU size.

Best regards

igor

View solution in original post

4 Replies
801 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chang

please look at

How to use KITL to debug i.mx53

also look at recommendations of WCE700_MX53_ER_1105_SMD_UserGuide.pdf

IMX53_TABLET_1105_WCE7_BSP_DOCS

-active / passive KITL modes of target i.MX53 (Eboot)

should meet host PC (Platform Builder) configuration.

If the SMD board is configured for active KITL, the image waits for a

Platform Builder connection before booting the OS image. Because the OS

image is already resident in Flash memory, it is necessary to reconfigure the

Platform Builder to jump directly to the image by selecting Target >

Connectivity Options > Core Service Settings > Download Image:

Never (jump to image).

-section 5.3 (Platform Builder Limitations/Issues):

Connection to Platform Builder Remote Tools may fail.

Workaround :

Network configuration for PC workstation may have MTU

(Maximum Transmit Size) size set to less than 1500, which is

not compatible with the KITL MTU size.

Best regards

igor

800 Views
changhsin-wen
Contributor II

Hello Igor,

Thank you for kindly advice :smileylaugh: ! I've reading your  useful information and after change eboot and set KITL work mode as interrupt, enable KITL enable mode  and finally success:smileylaugh: !!

But when start remote tool like FileViewer, it end up restart like following :smileycry:  anyone encounter the same problem as I do?

1.png

5.png

2.png

Sincerely,

Chang

0 Kudos
800 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chang

probably it is more suitable to post this to microsoft FAQ forum,

like below

USB KITL and USB OTG driver conflict

~igor

800 Views
changhsin-wen
Contributor II

Hi igor,

I read your post and change MTU size, but Remote tool still error  in message 0xC000005 and I connect device through Ethernet (via switch).

Truly grateful for your sharing and advice, I'll try to post to microsoft FAQ too :smileylaugh:. Wish you have a nice day !

6.png

Sincerely,

Chang

0 Kudos