Help the newbie get started

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help the newbie get started

2,585 次查看
danix
Contributor III
Hey, I saw the i.MX23 a while ago and thought it would be a perfect horse for my next ride. So I built a custom board in a mobile form factor, based on the reference schematic, and my PCB is delivered. Now, I'm not that good at software, but I want to know what is the easiest and quickest way to write a small code (blinking an LED), download to the processor and clap as the LED toggles :-) Any help is warmly appreciated!
标记 (1)
0 项奖励
回复
4 回复数

2,486 次查看
powerplay
Contributor I

Hi Kevin

I am newbie and I am working chumby hacker board

can I instaling this files to Hacker board if yes how I can do it whit my ubuntu 10.10 machine

I want to use cfimager exe  in XP return error

so  manually prepare make bootables sd card is very difficult so evertime I gave error code from imx23

(no mbr found)

I think I need bootable sd card .img file for writing win32 disk imager program

or which way I follow

 

best regards

0 项奖励
回复

2,486 次查看
KevinAnderle
Contributor II
Okay so then I would go here http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX23SDK_V0912&nodeId=0162468rH31143Z... This will give you the source for the boot loader and documentation. You will also need tools do do what you're trying. Do you have a tool yet? There is a JTag tool forum within the iMX Community you can go to for info on tools. Let me know if this helps get you going.
0 项奖励
回复

2,486 次查看
danix
Contributor III
Thanks Kevin. I've seen that application report, but I'm not familiar with the Linux platform...that is something I'll work on for the full project. Like I said, I just wanted to demonstrate my board by blinking an LED. so I need a quick way to write a simple code on windows and download to the board...

Kevin Anderle said:
I would start here...

http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf?fpsp=1... Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

Let me know if you need more help.
0 项奖励
回复

2,486 次查看
KevinAnderle
Contributor II
I would start here... http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation Let me know if you need more help.
0 项奖励
回复