Having trouble with mfg-tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Having trouble with mfg-tool

4,142件の閲覧回数
jsherman10
Contributor I

Hello, I just purchased a imx6-qp and I'm trying to load Android 5.0.0 for a research project. I have downloaded the prebuilt core image and the mfg tool.  I then extracted the images to the appropriate directory according to the quick start guide ( switched the board to download mode and connected the usb cable to the otg port).  I'm trying to boot Android from the SD Card.  I ran the correct .vbs file and it clicked on start and it seems to be stuck on loading u-boot. Any thoughts?

ラベル(5)
0 件の賞賛
返信
10 返答(返信)

3,658件の閲覧回数
mike_susen
NXP Employee
NXP Employee

I have one another point. You are using Android 5.0.0 but this is not supported by Quad+ chip. i.MX6QP is supported since Android 6.0. So please use Android 6.0 Instead of 5.0.0.

Michal

0 件の賞賛
返信

3,658件の閲覧回数
mike_susen
NXP Employee
NXP Employee

No, If you writing image to eMMC SD card does not need to be presented. And what about 8pin DIP switch configuration? Did you configure it correctly?

0 件の賞賛
返信

3,658件の閲覧回数
mike_susen
NXP Employee
NXP Employee

If I see your log, there is 1024bytes per block. Please use another card.

Michal

0 件の賞賛
返信

3,658件の閲覧回数
jsherman10
Contributor I

Okay, I also tried to use the MFG Tool to boot from EMMC as well, and I was still getting the same error.  Does the SD Card need to be present on the board even if I download the images to EMMC?

0 件の賞賛
返信

3,658件の閲覧回数
mike_susen
NXP Employee
NXP Employee

I'm using this tool SD Card Formatter - SD Association  under windows. MfgTool formats SD card automatically when you loading new image but there might be problem with your 32GB SD card.

Michal

0 件の賞賛
返信

3,658件の閲覧回数
jsherman10
Contributor I

Okay, I've also tried to partition the card using Linux and running the mksdcard-android sript, and I get the following error:

1+0 records in

1+0 records out

1024 bytes (1.0 kB) copied, 0.000261848 s, 3.9 MB/s

Checking that no-one is using this disk right now ...

BLKRRPART: Device or resource busy

This disk is currently in use - repartitioning is probably a bad idea.

Umount all file systems, and swapoff all swap partitions on this disk.

Use the --no-reread flag to suppress this check.

Disk /dev/sdc: 29476 cylinders, 64 heads, 32 sectors/track

sfdisk: ERROR: sector 0 does not have an msdos signature

/dev/sdc: unrecognized partition table type

Old situation:

No partitions found

Warning: given size (28412) exceeds max allowable size (28372)

New situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

   Device Boot Start   End    MiB    #blocks   Id  System

/dev/sdc1         0+    15     16-     16383+  83  Linux

/dev/sdc2        16     23      8       8192   83  Linux

/dev/sdc3        24   1103   1080    1105920    5  Extended

/dev/sdc4      1104  29515  28412   29093888   83  Linux

/dev/sdc5        24+   535    512-    524287+  83  Linux

/dev/sdc6       536+  1047    512-    524287+  83  Linux

/dev/sdc7      1048+  1055      8-      8191+  83  Linux

/dev/sdc8      1056+  1061      6-      6143+  83  Linux

/dev/sdc9      1062+  1063      2-      2047+  83  Linux

Warning: partition 4 extends past end of disk

Successfully wrote the new partition table

Re-reading the partition table ...

BLKRRPART: Device or resource busy

The command to re-read the partition table failed.

Run partprobe(8), kpartx(8) or reboot your system now,

before using mkfs

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)

to zero the first 512 bytes:  dd if=/dev/zero of=/dev/foo7 bs=512 count=1

(See fdisk(8).)

Checking that no-one is using this disk right now ...

BLKRRPART: Device or resource busy

This disk is currently in use - repartitioning is probably a bad idea.

Umount all file systems, and swapoff all swap partitions on this disk.

Use the --no-reread flag to suppress this check.

Disk /dev/sdc: 29476 cylinders, 64 heads, 32 sectors/track

Old situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

   Device Boot Start   End    MiB    #blocks   Id  System

/dev/sdc1         0+    15     16-     16383+  83  Linux

/dev/sdc2        16     23      8       8192   83  Linux

/dev/sdc3        24   1103   1080    1105920    5  Extended

/dev/sdc4      1104  29515  28412   29093888   83  Linux

/dev/sdc5        24+   535    512-    524287+  83  Linux

/dev/sdc6       536+  1047    512-    524287+  83  Linux

/dev/sdc7      1048+  1055      8-      8191+  83  Linux

/dev/sdc8      1056+  1061      6-      6143+  83  Linux

/dev/sdc9      1062+  1063      2-      2047+  83  Linux

New situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

   Device Boot Start   End    MiB    #blocks   Id  System

/dev/sdc1         8     15      8       8192   83  Linux

/dev/sdc2        16     23      8       8192   83  Linux

/dev/sdc3        24   1103   1080    1105920    5  Extended

/dev/sdc4      1104  29515  28412   29093888   83  Linux

/dev/sdc5        24+   535    512-    524287+  83  Linux

/dev/sdc6       536+  1047    512-    524287+  83  Linux

/dev/sdc7      1048+  1055      8-      8191+  83  Linux

/dev/sdc8      1056+  1061      6-      6143+  83  Linux

/dev/sdc9      1062+  1063      2-      2047+  83  Linux

Warning: partition 4 extends past end of disk

Successfully wrote the new partition table

Re-reading the partition table ...

BLKRRPART: Device or resource busy

The command to re-read the partition table failed.

Run partprobe(8), kpartx(8) or reboot your system now,

before using mkfs

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)

to zero the first 512 bytes:  dd if=/dev/zero of=/dev/foo7 bs=512 count=1

(See fdisk(8).)

Do you think that could also because the SD Card could be potentially bad?

0 件の賞賛
返信

3,658件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Hi Jonathan,

there might be may cases why it don't work. Please check these:

     - size of SD card

     - lock switch on SD card

     - change SD card

     - correct slot for SD card

     - newest version of MfgTool

     - try to flash into NAND

Hope it helps.

Michal

0 件の賞賛
返信

3,658件の閲覧回数
jsherman10
Contributor I

The size of the SD card is 32 GB. The lock switch is not set.  The MFG tool I downloaded is android_ L5.0.0_1.0.0-ga_tools.tar.gz.

I'm running windows 8 and all of my USB slots are 3.0. Do you think that's what is causing the problem?

0 件の賞賛
返信

3,658件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Jonathan,

please try to use 4/8GB SD card. Make sure that SD card is formatted to 512Bytes per block.

Michal

0 件の賞賛
返信

3,658件の閲覧回数
jsherman10
Contributor I

Alright, and sorry I'm new to this, how can I format the SD Card to 512Bytes per block?

0 件の賞賛
返信