Have you facing problem with EDID?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Have you facing problem with EDID?

1,924 Views
ajithpv
Contributor V

Hi all,

        When I was working with HDMI receiver chip driver development, I faced problem with the E-EDID (Enhanced Extended display identification data), many times. Some times the EDID data which respect to the resolution may not proper, otherwise not work at all.

So I would like to give a helpful link below, which can help you to create your customized EDID setting!

http://www.lightware.eu/index.php/support/downloads/667-advanced-edid-editor-software

With this software, you can View/Modify/create the EDID which suitable for you. It also gives the sample EDID setting for the standard resolutions too.

Please note that, the above link is just an example. There may be a better tool which existing too.

If you know a better tool or other helpful link, please post it as reply to this discussion.

Thanks in advance,

Ajith P V

Tags (2)
0 Kudos
Reply
0 Replies