Harpoon without Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Harpoon without Linux

2,490 Views
simmania
Contributor IV

Hi,

When I look at the pictures about Harpoon it seems that Both Linux and other RTOS modules are running on top of Jailhouse Hypervisor. It also says:

"Enables a choice of RTOS’s to run within Jailhouse hypervisor environment on the Arm® Cortex®-A cores of NXP MPU’s."

So this implies Harpoon can be used without Linux. Is that correct?

0 Kudos
Reply
3 Replies

2,435 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Simmania:

From the Harpoon User's Guide: Linux is needed

danielchen_0-1746582449571.png

 

 

Regards

Daniel

0 Kudos
Reply

2,424 Views
simmania
Contributor IV

This text does not say that Linux is required. It says that both Linux and an RTOS can run in parallel on the Harpoon environment. That does not mean that Linux is mandatory.

0 Kudos
Reply

2,323 Views
danielchen
NXP TechSupport
NXP TechSupport

Thanks, but the doc says the system starts on Linux and the Jailhouse hypervisor partitions the hardware to run both Linux and the guest RTOS in parallel.

 

danielchen_1-1747703720860.png

 

0 Kudos
Reply