Hardware security module in i.MX8M mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware security module in i.MX8M mini

989 Views
Hardevsinh_Palaniya
Contributor III

Hi,

I am using i.MX8M mini with Linux BSP. But i have some query.

  1. Hardware security Module: I have requirement of hardware security module which is also able to provide security against any harmful threat from Wi-Fi or Ethernet port. I was using optiga trustm for this purpose in my older version. Is there any inbuilt module available for the same? If “yes”, Can you please provide application note or any other documents of it?

  2. Also, I found that many security functionalities like Trustzone, DRM ciphers, secure clock, e-Fuse Key Storage, Random Number and 32 KB Secure RAM are available in i.MX8M mini. Can you please provide user guide or application note for Linux for using these features?

Any assistance will be greatly appreciated.

Senior Embedded Engineer | [email protected] | www.siliconsignals.io
0 Kudos
Reply
0 Replies