Hi,
Is there any hardware video convertor is available in imx6qsabreauto board? I want to convert NV12 format to BGRx format. If I use videoconvert, the video is very slow.
I am using this pipeline :
appsrc name=src is-live=true typefind=true block=false do-timestamp=true format=GST_FORMAT_TIME ! h264parse ! vpudec ! queue max-size-buffers=3 max-size-time=0 ! videoconvert ! waylandsink sync=false.
Hi Joan,
I used imxvideoconvert_ipu (Long-name : IMX ipu Video Converter) in my pipeline. Like this,
gst-launch-1.0 filesrc location=/home/root/video_with_display.h264 ! h264parse ! vpudec ! video/x-raw, format=NV12 ! imxvideoconvert_ipu ! video/x-raw,format=RGB16 ! waylandsink -v
Here I used a h264 file as source,instead of appsrc.
But I got a black screen.
The waylandsink on my board supports only BGRA, BGRx, RGB16. So I tried all these formats, but output is black screen only.
Is it is a problem with ipu? How to check?
What to do to make waylandsink to accept NV12?
how about useing ximagesink? for example:
"gst-launch-1.0 videotestsrc ! video/x-raw,format=NV12 ! imxvideoconvert_{xxx} ! video/xraw,
format=RGB16 ! ximagesink display=:0"
xxx = ipu or g2d, you can test this command to chech conversion works or not on your board.
Hi Joan,
Ipu is working fine, issue is with wayland display. I dumped the output from ipu and played it. I have made a new post for this issue. Kindly look into that.
Here is the link : https://community.nxp.com/thread/458623