Hardware Cryptography in FreeRTOS (CAAM)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware Cryptography in FreeRTOS (CAAM)

1,451件の閲覧回数
timholland
Contributor I

We want to use the CAAM device from freeRTOS.

We are using an iMX7D and currently we have Sabre SD boards for prototyping.

Has anybody implemented a device driver or interface to the CAAM for hardware cryptography in freeRTOS?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,315件の閲覧回数
art
NXP Employee
NXP Employee

No, there is no CAAM driver for the i.MX7D M4 core FreeRTOS BSP has been implemented so far.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信