HY4635 touch controller not responding properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HY4635 touch controller not responding properly

4,210件の閲覧回数
karthikssk
Contributor I

Hi,

I am using a 7" LCD (800*480)display(RGB interface) with cap touch (I2C interface) and the touch controller used is HY4635 and IMX6 SOLO processor is used. So the response of the touch is not very accurate and when the values are read in terminal window most of the time it shows wrong (X,Y) values like out of bound. 

Only some times there is the response . we cannot  do the drag operation but once in a while just single touch will respond that to very slowly . 

Can anyone please suggest whats the issue?

Any driver changes that need to be done ?

タグ(1)
0 件の賞賛
返信
1 返信

3,281件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Karthik

one can test with linux driver provided by HY4635 vendor

http://www.hycontek.com/wp-content/uploads/Linux_driver_sample_code.zip 

and try to calibrate using guidelines on

Tweaking Froyo for Nitrogen Part 1: touch support - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信