HW_OCOTP_MAC0: no such file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HW_OCOTP_MAC0: no such file

1,187件の閲覧回数
abhinandan1
Contributor I

Hi all, I am trying to port project from thud to gatesgarth version. After making all the necessary changes, I tried writing the image on board, the device runs software update and tries to reboot. While rebooting it throws the following error

 

[TRACE] : SWUPDATE running : [install_single_image] : Found installer for stream boot.ext2.gz raw
[INFO ] : SWUPDATE successful !
./recovery.sh: line 190: can't open /sys/fsl_otp/HW_OCOTP_MAC0: no such file
Installation failed. Halting.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,
 
/sys/fsl_otp/HW_OCOTP_MACx was removed since we do not support export the fuse interface in the Linux console.

Best regards,
Aldo.

0 件の賞賛
返信