HFP Profile support for sabre sd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HFP Profile support for sabre sd

1,295件の閲覧回数
amit251291
Contributor IV

Hi,

We have a imx6q sabre SD board running on android 7.0

A WiFi/Bluetooth module is connected to provided SDIO interface & J13 cable connector. 

Default A2DP Sync app is working perfectly and im able to hear a streamed music on headset.

Now we want to interface Bluetooth HFP profiles so that even phone will get sync with it. 

What changes i have to do in software as well as in hardware to get it worked ? 

Board is running on Android 7.0

0 件の賞賛
返信
1 返信

1,167件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

According to our release notes, the HFP Profile is not supported. Furthermore, we cannot provide that kind of support. I apologize for the inconveniences.

Best Regards,

Diego.

0 件の賞賛
返信