IMX6Q USE 4PCS NT5CB256M16CP-DII as DRAM,how to config imx6q's register ,UBOOT FILE?
Hi liu
first please run ddr test
i.MX6/7 DDR Stress Test Tool V2.90
DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations.pdf
use attached Porting Guide
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI,IGO'
I HAVE DONE DDR STRESS TEST MONTH AGO,most time have problem DQS test error,BUT if write & read a single address ,i found this operation success,MAYBE BLOCK read /write failed,how can use softwaretool can make sure the CHIP IMX6Q having solder problem,SO as the two addr-pin have conneted?or pretended solder?
for solder problems one can test with jtag and oscilloscope or inspect layout using x-ray screening.
dear,
i found a problem,when i have fourteen pcs BOARD,some PCBS DDR DRESS TEST ,I CAN read/write single word (32bit) for single address,but DDR dress test some address write have wrong hex data,how to fine tune the register for writing sequence in time?