HDMI video doesn't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI video doesn't work

2,873件の閲覧回数
KenSnyder
Contributor I

I just received a QSB with an HDMI daughterboard.  With the distributed SD Card I was able to boot into Linux perfectly, however when I run the commands:

set bootargs_base 'bootargs console=ttymxc0,115200 ${hdmi}'

saveenv

boot

the board reboots and displays the Linux penguin in the upper left and then stops indefinitely.

Any ideas what I'm doing wrong? 

Thanks,

Ken Snyder

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,341件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

It´s always caused by some magic bootargs....

Nice to know it´s working

0 件の賞賛
返信

2,341件の閲覧回数
KenSnyder
Contributor I

Daiane,

Thanks for the info and feedback.  

I've got it working, probably more by happy accident than anything else.

PS: My /proc/cmdline is as follows:

console=ttymxc0,115200 gpu_nommu setenv bootargs console=ttymxc0,115200 video=mxcdi0fb:RGB24,1024x768M@60 hdmi di0_primary root=/dev/mmcblk0p1 rw rootwait

But as I mentioned, now it's working.

Thanks again,

Ken



Daiane Angolini said:

Can you share your bootargs, or even better, your cat /proc/cmdline

(I would like to see if your bootargs is being created the right way)

Do you get some error? Do you get the prompt?

0 件の賞賛
返信

2,341件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Can you share your bootargs, or even better, your cat /proc/cmdline

(I would like to see if your bootargs is being created the right way)

Do you get some error? Do you get the prompt?

0 件の賞賛
返信

2,341件の閲覧回数
KenSnyder
Contributor I

I spotted a typographical error but fixing it made no difference.

set bootargs_base 'set bootargs console=ttymxc0,115200 ${hdmi}'


Any help would be very much appreciated. Thx

0 件の賞賛
返信