HDMI clock gating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI clock gating

8,938 Views
nirmalluhana
Contributor IV

Hello,

 

Release: Yocto-Sumo (4.14.78_1.0.0_GA)

Board: i.MX8MQ based custom board

We are getting radiation from our board at 297 & 594 MHz frequencies, which is used by HDMI interface.

We want to disable DISPLAY_HDMI_CLK_ROOT on our board to stop the radiation of above frequencies. We already disabled HDMI interface from dts file.

Although, we are getting above clock frequencies and it is radiating due to PLL in the processor.

How we can completely disable the DISPLAY_HDMI_CLK_ROOT from PLL?

Best regards,

Nirmal

Labels (1)
Tags (2)
9 Replies

8,667 Views
igorpadykov
NXP Employee
NXP Employee

Hi NIRMAL

for disabling HDMI clocks one can try to use CCGR gating control (CCM_CCGR95, CCM_CCGR94),

described in Table 5-9. CCGR Mapping Table

i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

8,667 Views
nirmalluhana
Contributor IV

Hello Igor,

Thanks for your rapid response.

Can you please provide more information from where I can access these registers to override the values?

Best regards,

Nirmal

0 Kudos
Reply

8,667 Views
nirmalluhana
Contributor IV

Hello Igor,

 

Thanks for updates.

 

I didn't found clock source used for HDMI interface in the above-mentioned files.

Can you please provide which configurations I have to change to disable HDMI clock?

 

Best regards,

Nirmal

0 Kudos
Reply

8,667 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

one can printf ccm registers to find clock source.

Best regards
igor

8,667 Views
nirmalluhana
Contributor IV

Hello Igor,

 

Thanks for your response.

 

As per the "fsl-imx8mq.dtsi" file there is no HDMI specific clock is used for HDMI interface. It is used DCSS node clocks for HDMI interface.

So, how I can disable HDMI(CCM_CCGR94) & HDMI PHY(CCM_CCGR95) clocks?

In the above clock source file, there is information about display clocks which is used for the DCSS source. If I disable the clocks from that source file my new built kernel crashes while board boot up.

Can you please provide the solution to disable HDMI interface clock?

 

Best regards,

Nirmal

0 Kudos
Reply

8,660 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

>can you please provide the solution to disable HDMI interface clock?

suggest to build minimal image as described in Table 1. i.MX Yocto project images

attached Yocto Guide. Seems DCSS uses HDMI clock, so it is necessary to disable DCSS

also, use LCDIF instead:

fsl-imx8mq-evk-lcdif-adv7535.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

&dcss {
    status = "disabled";
};

&hdmi {
    status = "disabled";
};
 

Best regards
igor

0 Kudos
Reply

8,660 Views
nirmalluhana
Contributor IV

Hello Igor,

 

Thanks for your response.

 

I have disabled both the "dcss" & "hdmi" nodes in the dts file. But still, I am getting the radiation at 297 & 594 MHz frequencies. I think it is generated out from PLL of video clock.

I have also commented the line "clk_set_rate(clks[IMX8MQ_VIDEO_PLL1], 593999999);" in "drivers/clk/imx/clk-imx8mq.c" clock source file which is set the clock frequency at 594 MHz. But, it is not worked.

So, Is there any other changes I have to take care to disable HDMI interface clock?

 

Best regards,

Nirmal

0 Kudos
Reply

8,660 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

to trace source of noise one can attach jtag and set PLL_BYPASS bit

in CCM_ANALOG_x_PLLn_CFG0 registers, check if radiation persists.

Best regards
igor

0 Kudos
Reply