HDMI Video is not ready!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI Video is not ready!

Jump to solution
7,254 Views
nirmaltm
Contributor II

Dear All,

I am using iMX6 Sabre Auto board for GENIVI platform making.. For developing the image i have used the help from meta-fls-ivi and the Yocto build. the GENIVI 7.0 build was successfully done. But while booting the sdcard image the flowing error has occur.

____________________________________________________________________________

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

[  OK  ] Reached target Multi-User System.

         Starting Update UTMP about System Runlevel Changes...

[FAILED] Failed to start Bluetooth service.

See 'systemctl status bluetooth.service' for details.

         Starting WPA supplicant...

[  OK  ] Started Update UTMP about System Runlevel Changes.

[  OK  ] Started WPA supplicant.

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

Yocto GENIVI Baseline (Poky/meta-ivi) 7.0.3 imx6qsabreauto ttymxc3

___________________________________________________________________________________

The system is starting in to init after this error. but the HDMI is not working.

I have gone through many post regarding the same error. but the result is same. when I change the boot configuration as :

mxcfb0:dev=hdmi,1280x720M@60, if=RGB24.

The system is stuck while booting. the kernal is not loading in this time. I think the system suspend the console

So, i have added the consoleblank=0. but the result was same.

kindly help me to resolve this problem.

0 Kudos
Reply
1 Solution
4,392 Views
nirmaltm
Contributor II

Hi all,

Thanks for your help, the problem is solved by changing the u-boot by newer version (uboot-imx-imx_v2015.04_3.14.52_1.1.0_ga). I think the error -22 is for invalid parameter. the previous u-boot is sending a bad parameter for loading the kernal. so when a HDMI is needed it shows the error. After changing the U-boot the error is not showing as well as the HDMI is working properly.

Thanks

View solution in original post

0 Kudos
Reply
5 Replies
4,393 Views
nirmaltm
Contributor II

Hi all,

Thanks for your help, the problem is solved by changing the u-boot by newer version (uboot-imx-imx_v2015.04_3.14.52_1.1.0_ga). I think the error -22 is for invalid parameter. the previous u-boot is sending a bad parameter for loading the kernal. so when a HDMI is needed it shows the error. After changing the U-boot the error is not showing as well as the HDMI is working properly.

Thanks

0 Kudos
Reply
4,392 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

could you run cat /sys/class/graphics/fb0/modes

to check what modes are supported. Also if HDMI is enabled

in u-boot, could you try to disable it in u-boot.

Had you tried with 1920x1080 HDMI  and other monitors?

Best regards

igor

0 Kudos
Reply
4,392 Views
nirmaltm
Contributor II

Thanks igor,

I have tired the above mention activities the results as follows :

1. cat /sys/class/graphics/fb0/modes :

Yocto GENIVI Baseline (Poky/meta-ivi) 7.0.3 imx6qsabreauto ttymxc3

imx6qsabreauto login: root

Password:

root@imx6qsabreauto:~# cat /sys/class/g

gpio/            graphics/        graphics_class/

root@imx6qsabreauto:~# cat /sys/class/graphics/fb

fb0/    fb1/    fb2/    fb3/    fb4/    fbcon/

root@imx6qsabreauto:~# cat /sys/class/graphics/fb0/

bits_per_pixel         fsl_disp_property      state

blank                  mode                   stride

console                modes                  subsystem/

cursor                 name                   uevent

dev                    pan                    virtual_size

device/                power/

fsl_disp_dev_property  rotate

root@imx6qsabreauto:~# cat /sys/class/graphics/fb0/mode

D:1024x768p-60

root@imx6qsabreauto:~#

2. HDMI is disabled in u-boot

the result was same. we got an HDMI error while kernel loading.

3. Tried with different monitors with Full HD as well

but the result was same.

kindly help me to avoid this HDMI error

0 Kudos
Reply
4,392 Views
igorpadykov
NXP Employee
NXP Employee

you can check if this hdmi resolution is supported, as in

example below "mxcfb2: fb@1 "

linux-2.6-imx.git - Freescale i.MX Linux Tree

0 Kudos
Reply
4,392 Views
nirmaltm
Contributor II

Dear igor,

I have tried the above but the result is same. the error is not going as well as HDMI is not working

0 Kudos
Reply