HDMI TX PHY Databook

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,284件の閲覧回数
endl
Contributor II

Hello

Where can I find the "DesignWare Cores HDMI TX PHY Databook" and PHY datasheet for IMX6DL HDMI Tx PHY ?

Thanks in advance.

ラベル(2)
0 件の賞賛
返信
1 解決策
3,702件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

you can request it from synopsys

DesignWare HDMI Transmitter

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,703件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

you can request it from synopsys

DesignWare HDMI Transmitter

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,700件の閲覧回数
tommalnar
Contributor III

I attempted to contact synopsys and they said we need a site ID.  I asked how to obtain a site ID and they said NXP must provide theirs.  Seems to be a painful circle here to try and get HDMI or HDMI Phy docs.  Is there any chance NXP can publish them?

0 件の賞賛
返信
3,702件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

really the Synopsis specs are very close to  Chapter 33 [HDMI Transmitter (HDMI)]
and  Chapter 34 [HDMI 3D Tx PHY (HDMI_PHY)] of the i.MX6 D/Q RM (IMX6DQRM,
Rev. 3, 07/2015). Some unpublished  details may be considered in NXP requests.

1)     Please open www.nxp.com

2)     On the top level menu, select  
           Support > Sales and Support (http://www.nxp.com/support/sales-and-support:SUPPORTHOME).

3)     On the bottom of the page, select Hardware & Software.

4)     Register with your business email to access the technical NXP online support.

5)     A verification email will be sent to your account. Click the embedded link to verify your access.

6)     On the NXP online support page, select Contact Support from the top menu and click “submit a new case”  
        to start the process.

Regards,

Yuri.

0 件の賞賛
返信