HDMI Display issue in iMX6DP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI Display issue in iMX6DP

1,606件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team

Our platform is follow IMX6DP demoboad.

In HDMI, our panel will be show noise signal.  (Picture)

The log message in dmesg&fbi.txt

Do you have any idea to fixed the display issue?

 

charleshuang_0-1665025432228.png

 

About ipu log 

root@imx6q-dms-ba16:~# dmesg | grep ipu
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
root@imx6q-dms-ba16:~# dmesg | grep pre
L2C-310 ID prefetch enabled, offset 16 lines
DMA: preallocated 256 KiB pool for atomic coherent allocations
imx-pre 21c8000.pre: driver probed
imx-pre 21c9000.pre: driver probed
imx-pre 21ca000.pre: driver probed
imx-pre 21cb000.pre: driver probed
pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref]
pci 0000:01:00.0: reg 0x30: [mem 0x00000000-0x000fffff pref]
pci 0000:00:00.0: BAR 9: assigned [mem 0x01300000-0x013fffff pref]
pci 0000:00:00.0: BAR 6: assigned [mem 0x01400000-0x0140ffff pref]
pci 0000:01:00.0: BAR 6: assigned [mem 0x01300000-0x013fffff pref]
pci 0000:00:00.0: bridge window [mem 0x01300000-0x013fffff pref]
imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update

ラベル(1)
0 件の賞賛
返信
0 返答(返信)