HABv4 vs. AHAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HABv4 vs. AHAB

2,938件の閲覧回数
ravindrajinka88
Contributor I

I can able to See Secure boot related stuff in both AHAB and HABv4, How can i select which is required in my project.

Please let me know the exact difference between HABv4 and AHAB.

Thanks in advance.

0 件の賞賛
返信
2 返答(返信)

2,837件の閲覧回数
ravindrajinka88
Contributor I

Thanks Yuri

0 件の賞賛
返信

2,837件の閲覧回数
Yuri
NXP Employee
NXP Employee

 

Hello,

 

   i.MX 50, i.MX 53, i.MX 6, i.MX 7 and i.MX8M Series are using HABv4.

i.MX8 and i.MX8X are using AHAB.

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.