HABv4 PKI - CA Required?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HABv4 PKI - CA Required?

2,162 Views
mprt42
Contributor III

Hi,

I have a some general question about the HABv4 PKI concepts.

1) Why is a CA required? Why do the SRK Certificates have to be signed by the CA?
The fuses just contain the hash of the SRK table, right? so the four SRKs can just be root certificates as well, no? Also, there seems to be no need for the four SRKs to be signed by the same CA, no?

 

2) What's the usecase of the add_key script?
When would I use that?
I generate the SRKs, burn the fuses and after that things are set in stone, no?

 

3) What would be the usecase for someone *not* to use all 4 SRK slots in the table?
e.g. why would someone fuse a SRK table with just a single entry?
What happens should that key index at some point being revoked/fused ?

 

Thanks a lot!

 

 

0 Kudos
Reply
3 Replies

2,141 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

-> SGK is issued by SRK, the CA of SGK is SRK. CA is the holder of a private key used to certify public keys, the SRK private key is held by the CA.

-> Generally used to add new SGK. It is also possible to replace the OpenSSL and the hab4_pki_tree script with an alternative key generation solution,

-> Only one of the SRKs in the table may be selected for use on the NXP processor per reset cycle.

 

Regards

Harvey

0 Kudos
Reply

1,884 Views
mprt42
Contributor III

Hi Harvey,

thanks for your answer.
Unfortunately, it does not answer my questions.
Could you please answer my questions?
I have not asked about SGK.

Thanks a lot!

0 Kudos
Reply

2,065 Views
opedis
Contributor III

Where does SGK come from for HABv4 PKI?

$ ./hab4_pki_tree.sh
  ...
  Do you want to use an existing CA key (y/n)?: n
  Do you want to use Elliptic Curve Cryptography (y/n)?: n
  Enter key length in bits for PKI tree: 2048
  Enter PKI tree duration (years): 5
  How many Super Root Keys should be generated? 4
  Do you want the SRK certificates to have the CA flag set? (y/n)?: y

The diagram below illustrate the PKI tree:

                                +---------+
                                |   CA    |
                                +---------+
                                     |
                                     |
            ---------------------------------------------------
            |               |                 |               |
            |               |                 |               |
            v               v                 v               v
       +--------+       +--------+       +--------+       +--------+
       |  SRK1  |       |  SRK2  |       |  SRK3  |       |  SRK4  |
       +--------+       +--------+       +--------+       +--------+
         /    \           /    \           /    \           /    \
        v      v         v      v         v      v         v      v
     +----+  +----+   +----+  +----+   +----+  +----+   +----+  +----+
     |CSF1|  |IMG1|   |CSF2|  |IMG2|   |CSF3|  |IMG3|   |CSF4|  |IMG4|
     +----+  +----+   +----+  +----+   +----+  +----+   +----+  +----+

After running the script users can check the private keys under keys/ directory
and their respective X.509v3 public key certificates under crts/ directory.
Those files will be used during the signing and authentication process.

2.1 Generating a fast authentication PKI tree
----------------------------------------------

Starting in HAB v4.1.2 users can use a single SRK key to authenticate the both
CSF and IMG contents. This reduces the number of key pair authentications that
must occur during the ROM/HAB boot stage, thus providing a faster boot process.

The script hab4_pki_tree.sh is also able to generate a Public Key Infrastructure
(PKI) tree which only contains SRK Keys, users should not set the CA flag when
generating the SRK certificates.

- Generating 2048-bit fast authentication PKI tree on CST (starting from
v3.1.0):

  $ ./hab4_pki_tree.sh
  ...
  Do you want to use an existing CA key (y/n)?: n
  Do you want to use Elliptic Curve Cryptography (y/n)?: n
  Enter key length in bits for PKI tree: 2048
  Enter PKI tree duration (years): 5
  How many Super Root Keys should be generated? 4
  Do you want the SRK certificates to have the CA flag set? (y/n)?: n

The diagram below illustrate the PKI tree generated:

                             +---------+
                             |   CA    |
                             +---------+
                                  |
                                  |
         ---------------------------------------------------
         |               |                 |               |
         |               |                 |               |
         v               v                 v               v
    +--------+       +--------+       +--------+       +--------+
    |  SRK1  |       |  SRK2  |       |  SRK3  |       |  SRK4  |
    +--------+       +--------+       +--------+       +--------+
0 Kudos
Reply