HABv4: Authenticated image running XIP from serial flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HABv4: Authenticated image running XIP from serial flash

Jump to solution
1,868 Views
spiderman
Contributor III

Suppose I am using a processor with HAB (High Assurance Boot) v4. It is i.MX RT1062, but the same can be considered for other processors with HAB as well.

Let's say I execute in place (XIP) from serial flash a signed (but not encrypted) bootable image. Therefore the HAB code in ROM should check the signature before running the application.

However, is there some mechanism preventing that someone implements spoofing on the serial bus from the flash, and thus injecting a "jump" to some malware firmware on some other area of the flash? Or even substitute instructions from inside my bootable image area?

 

0 Kudos
Reply
1 Solution
1,827 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @spiderman ,

There are three security boot level, HAB boot, HAB encrypted boot and OTFAD encrypted boot.

If it is only HAB boot, it can't prevent this kind of attack. HAB boot only verify the image is authentic. But after that, the right of control is pass to application. To prevent this attack, you can run in internal SRAM instead of XIP. HAB encrypted boot doesn't support XIP because the image is encrypted.

OTFAD is a hardware which can decrypt on-the-fly. So, the data on the SPI bus is encrypted. It can prevent such attack when XIP.

 

Regards,

Jing 

View solution in original post

0 Kudos
Reply
1 Reply
1,828 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @spiderman ,

There are three security boot level, HAB boot, HAB encrypted boot and OTFAD encrypted boot.

If it is only HAB boot, it can't prevent this kind of attack. HAB boot only verify the image is authentic. But after that, the right of control is pass to application. To prevent this attack, you can run in internal SRAM instead of XIP. HAB encrypted boot doesn't support XIP because the image is encrypted.

OTFAD is a hardware which can decrypt on-the-fly. So, the data on the SPI bus is encrypted. It can prevent such attack when XIP.

 

Regards,

Jing 

0 Kudos
Reply