Gstreamer network decoding performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer network decoding performance

1,869 Views
timothybean1
Contributor I

Hello all,

I have just purchased a new Nitrogen6x board for testing. My application is a low latency HD decoder. I am interested if anyone can comment as to the latency of decoding a 720p H.264 video stream from the network (RTSP). I would like to know what the expected latency is out-of-the box for the Freescale Gstreamer elements. I have been digging around and found a min_latency setting for the vpudec element that looks like something I would want to use. Can anyone give me some expectations. I am looking for less than 500 ms end-to-end. Is that feasible without modification to the Gstreamer elements?

Thanks

Tim

Labels (3)
1 Reply

1,614 Views
timothybean
Contributor IV

The network streaming is very good. Latency is excellent.