Gstreamer-1.x and FSL plugins with Linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer-1.x and FSL plugins with Linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?

1,581 Views
RobbieJiang
Contributor IV

Hi,

I'm currently working with MX6Q and Ltib L3.0.35_4.1.0.

The gstreamer included in L3.0.35_4.1.0 is 0.1x and I would like to switch to gstreamer-1.x.

Seems that fsl-L3.14.28_1.0.0_iMX6qdls_Bundle comes with gstreamer-1.x.

But I do not want to change my kernel and drivers.

So is there a way to use gstreamer-1.x and the corresponding FSL video plugins with linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?

Thanks,

Robbie

Labels (3)
0 Kudos
Reply
1 Reply

1,162 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

I am afraid this is not possible, since plugins are compiled for

specific kernel, as discussed below

GStreamer i.MX6 Pipelines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply