Getting started with i.MX 28 EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started with i.MX 28 EVK

ソリューションへジャンプ
3,510件の閲覧回数
engine
Contributor I

Hi!

I've got aan i.MX28 EVK, and I have to implement a whole bunch of C programs, for that I need to run at least a 'hello world', for that I get would to format the SD card with the newst OS and using a PUTTY writing the program that I need, my problem is that I don't find a documentation that can help me do that . can anybody help me with that, I'll be thankfull1

Best regards!

ラベル(2)
0 件の賞賛
返信
1 解決策
3,360件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Freescale does not have Debian Root File System available.  But we have Ubuntu for our boards, but it should be just to get the package from Debian.and use our Kernel to have the board up and running.

FYI. You have also  GNOME graphic interface in the Linux BSP package which I think can be also a another option for you


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,360件の閲覧回数
ganeshh
Contributor III

Hello engine

Follow this link

https://community.freescale.com/docs/DOC-93394

It describes and provides the links to download BSP Source and DOCs

3,360件の閲覧回数
engine
Contributor I

@Ganesh H ,

thanks a lot for your answer , is it possible to get debian on the board ?

0 件の賞賛
返信
3,361件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Freescale does not have Debian Root File System available.  But we have Ubuntu for our boards, but it should be just to get the package from Debian.and use our Kernel to have the board up and running.

FYI. You have also  GNOME graphic interface in the Linux BSP package which I think can be also a another option for you


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,360件の閲覧回数
ganeshh
Contributor III

engine

No idea about that..