Getting "Synchronous Abort" handler error in IMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting "Synchronous Abort" handler error in IMX8QM

4,710 次查看
vinothkumars
Senior Contributor IV

Hi All,

 

I got following error and I unable to find out the address (00000000789f0000) from .map file.

 

U-Boot SPL 2018.03-00003-g0d0fb52-dirty (Aug 20 2021 - 18:19:27 +0530)
Trying to boot from MMC1
Authentication key not yet programmed
keyslot package magic error, do nothing here!
Authentication key not yet programmed
Booting from bootloader_a...U
welcome to lk/MP

boot args 0x2000000 0xfe000000 0x2000 0x0
generic_arm64_map_regs: failed -5 name=gic
initializing trusty (Built: 17:00:46 Mar 5 2019)
Initializing Trusted OS SMC handler
int rebuild_hset_all(struct uctx *):238: Rebuilding all handles set
hwcrypto: 222: Initializing
hwrng_caam: 44: Init HWRNG service provider
hwrng_srv: 256: Start HWRNG service
int rebuild_hset_all(struct uctx *):238: Rebuilding all handles set
hwcrypto_caam: 78: Init HWCRYPTO service provider
hwcrypto_srv: 306: Start HWCRYPTO service
hwkey_caam: 169: Init HWKEY service provider
hwkey_caam: 138: Invalid magic
hwkey_srv: 331: Start HWKEY service
hwcrypto: 237: enter main event loop
int rebuild_hset_all(struct uctx *):238: Rebuilding all handles set
int rebuild_hset_all(struct uctx *):238: Rebuilding all handles set
int rebuild_hset_all(struct uctx *):238: Rebuilding all handles set
MMC: FSL_SDHC: 0
In: serial@5a060000
Out: serial@5a060000
Err: serial@5a060000
flash target is MMC:0
libtipc.c: INFO Initializing Trusty device
trusty_dev.c: INFO selected trusty api version: 3 (requested 3)
libtipc.c: INFO Initializing Trusty IPC device
libtipc.c: INFO Initializing RPMB storage proxy service
ss: get_rpmb_auth_key: failed to get key: -2
ss: proxy_connect: can't get storage auth key: (-2)
ipc: do_connect: failure initializing channel state (1001)
rpmb_proxy.c:312: ERROR rpmb_storage_proxy_init: unexpected proxy channel close
libtipc.c:93: ERROR Initlializing RPMB storage proxy service failed (-8)
Authentication key not yet programmed
libtipc.c: INFO Initializing Trusty Hardware Crypto client
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
Verifying slot _a ...
avb_vbmeta_image.c:206: ERROR: Hash does not match!
avb_slot_verify.c:692: ERROR: vbmeta_a: Error verifying vbmeta image: HASH_MISMATCH
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed
avb_slot_verify.c:388: ERROR: boot_a: Hash of data does not match digest in descriptor.
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
verify FAIL, state: UNLOCK
boot 'boot_a' still
Kernel load addr 0x80280000 size 9010 KiB
kernel @ 80280000 (9225875)
ramdisk @ 83400000 (2588437)
fdt @ 83200000 (104058)
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
ERROR - failed to read public key for keymaster
keymaster.c:318: ERROR Keymaster TIPC client not initialized!
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
ipc_dev.c:306: ERROR trusty_ipc_dev_close: secure OS returned (-7)
## Flattened Device Tree blob at 83200000
Booting using the fdt blob at 0x83200000
Using Device Tree in place at 0000000083200000, end 000000008321c679
/dma-controller@5a1f0000, 71520
/dma-controller@591F0000, 72312
/dma-controller@591F0000, 72312
/dma-controller@599F0000, 73288

Starting kernel ...

"Synchronous Abort" handler, esr 0x02000000
elr: 00000000789f0000 lr : 0000000080021b08 (reloc)
elr: 0000000081090000 lr : 00000000886c1b08
x0 : 0000000083200000 x1 : 0000000000000000
x2 : 0000000000000000 x3 : 0000000000000000
x4 : 0000000080280000 x5 : 0000000000000001
x6 : 0000000000000008 x7 : 0000000000000000
x8 : 000000008873c328 x9 : 0000000000000002
x10: 000000000a200023 x11: 0000000000000002
x12: 0000000000000002 x13: 0000000083abdd8e
x14: 00000000843a8ea2 x15: 00000000886c1244
x16: 000000008227fff7 x17: 0000000000000000
x18: 0000000083abdd78 x19: 000000008873c170
x20: 0000000000000000 x21: 0000000083aae9b8
x22: 0000000000000003 x23: 0000000083aae9b8
x24: 0000000000000000 x25: 0000000000000000
x26: 0000000000000000 x27: 00000000886c1b14
x28: 0000000000000000 x29: 0000000083aae780

Resetting CPU ...

resetting ...

 

 

 

 

Regards,
Vinothkumar Sekar
0 项奖励
回复
7 回复数

4,698 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

one can try to debug it using AN12631  AN12631: Normal and Secure Debug for i.MX8/8X Family of Applications Processors – Application Note

 

Best regards
igor

0 项奖励
回复

4,690 次查看
vinothkumars
Senior Contributor IV

Thank you Igor for the reply.

 

But, I unable to debug using this document.

Will you please give some more information what exactly happens here ?

 

Regards,
Vinothkumar Sekar
0 项奖励
回复

4,687 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

4,681 次查看
vinothkumars
Senior Contributor IV

Yes Igor

 

Please find the test report,

 

 

Regards,
Vinothkumar Sekar
0 项奖励
回复

4,665 次查看
vinothkumars
Senior Contributor IV

Hi @igorpadykov ,

 

This error I observed after sometime from power off to power on and not in all time.

And also address are start from 0x80000000 but here the error appends from 

789f0000

 

 

 

 

Regards,
Vinothkumar Sekar
0 项奖励
回复

4,661 次查看
igorpadykov
NXP Employee
NXP Employee

>This error I observed after sometime from power off to power on..

 

please check below requirement

 

1.jpg

Best regards
igor

0 项奖励
回复

4,646 次查看
vinothkumars
Senior Contributor IV

Thank you Igor for the reply.

 

Instead of power off the board I tried "shutdown" from command line and the device power off take sometime compare to normal on and off. but, still I faced same error.

 

And also I measure all voltage source all in 0 v only

 

Regards,
Vinothkumar Sekar
0 项奖励
回复