Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?

5,849 次查看
sivaalagarsamy
Contributor II

The u-boot has a board configuration file which has DCD data in the following format.

ADDRESS-TYPE  ADDRESS  VALUE

I am using the IOMux Tool to configure the IOMUX.

Is there a easy way to generate the DCD data from the IOMux Tool?

Thanks,

Siva

标签 (2)
标记 (2)
0 项奖励
回复
4 回复数

3,136 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Siva

there is no way for automatic DCD generation from

IOMUX tool.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,136 次查看
mchaplet
Contributor II

Hi,

Is there another way to generate DCD data ?

Do you have examples DCD for various DDR hardware configurations or an application note dealing with ?

Mine is single chip MT41K128M16 (16M*16*8banks = 256MB) and I try to load correct configuration without success for the moment ...

Thanks,

Martin

0 项奖励
回复

3,136 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

3,136 次查看
mchaplet
Contributor II

Thanks, It helps a lot !

As a note, for other new designs : Don't forget to use MX6_MMDC_P0_MPODTCTRL = 0x00011117  instead default 22227 generated by script aid XLS.

I've found it "recommanded for new designs" in MX6DL_SabreSD_DDR3_register_programming_aid_v1.5.inc

0 项奖励
回复