Generating a clock on SSP2_SCK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generating a clock on SSP2_SCK

1,561件の閲覧回数
danbocko
Fresh Out Contributor

I have been trying to configure an i.MX287 to generate a clock on SSP2_SCK with no success. I used the OBDS as a starting point. I have also been reading Section 10 of the i.MX28 Applications Processor Reference Manual, this is from section 10.2.3;

"This clock gating is instantiated using an ICG element from the standard cell library."

What is an ICG element and how do I use it? An Internet search provided no useful information. 

Thanks

Dan

ラベル(1)
0 件の賞賛
返信
1 返信

1,478件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dan

on i.MX28 EVK this signal is used for spi-nor and one can look at patches on

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信