General questions regarding Qvfb on Embedded Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

General questions regarding Qvfb on Embedded Linux

1,714件の閲覧回数
bonil
Contributor I
I've read a lot of interesting posts and articles about virtual framebuffer and how to use it, but I'm still unclear as to what I can do for me, leading me to ask a few questions:
  1. Does the virtual framebuffer work only with X Window System? Does it mean that when using qt-embedded.spec, available in the LTIB, qvfb will not work?
  2. Is it correct to say that Qvfb allow to run an application on the target and display the application gui on the host and use keyboard + mouse of the host? That means that qvfb will always run on the host?
タグ(2)
0 件の賞賛
返信
1 返信

1,632件の閲覧回数
katte
Contributor II

I don't use qvfb, maybe I'm wrong, but i think that it is a tool that run on x-window system for simulate the resolution and the parameter of the target, but all is running on the host.

0 件の賞賛
返信