Gen II .wf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gen II .wf

1,412件の閲覧回数
ekerebel
Contributor III

I have the i.MX 6SLL dev board with the EBOOKDC4 EPD board.

Can you provide updated .wf to leverage the Reagl/- D Support (Gen II)?

0 件の賞賛
返信
1 返信

1,376件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Erwan Kerebel,

Are you interested in a specific BSP Release? If the Regal/Regal-D algorithms are needed, the Regal/Regal-D algorithm patches must be applied to the basic BSP. The last BSP I checked that had these as controlled access packages on the Release Notes is L4.9.88_2.0.0, these controlled packages are available through a marketing representative or Distributor.

Beside these patches the waveform would also change for the Regal/Regal-D algorithms from the usual 4-bit to a 5-bit pixel waveform. This should be provided by EInk as part of the support to their panels. Once you have this waveform you may open a Case asking for it to be parsed for the i.MX6SLL, but you would still need the patched BSP so that the driver can understand this waveform.

Regards,

0 件の賞賛
返信