GUI Image with buildroot for IMX8MM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI Image with buildroot for IMX8MM

Jump to solution
3,795 Views
kanakshilledar
Contributor II

Hi,

I am trying to develop a GUI image for IMX8MM using buildroot. 

Are there any reference defconfigs for such example? If not what are the major packages to be selected while building? I want to build on wayland.

 

Thanks!

0 Kudos
Reply
1 Solution
3,636 Views
gary_bisson
Senior Contributor III

Hi,

You can use the configuration below meant for Ezurio devices:

https://github.com/boundarydevices/buildroot-external-boundary/blob/master/configs/nitrogen8mm_qt5_g...

It includes weston & qt.

Regards

View solution in original post

8 Replies
3,765 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @kanakshilledar 

I hope you are doing very well.

 

Unfortunately there are not buildroot examples. At this moment we just provide support to Yocto.

 

Best regards,

Salas.

0 Kudos
Reply
3,750 Views
kanakshilledar
Contributor II

Hello @Manuel_Salas 

I’m doing well—hope you are too!

Unfortunately there are not buildroot examples.

Thank you for the clarification. Since there are no official Buildroot examples, I wanted to ask: I noticed there are some i.MX8MM-related defconfigs in the Buildroot tree. Are these community-maintained, or contributed by NXP at some point?

Best Regards

 

0 Kudos
Reply
3,726 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @kanakshilledar 

Could you please share the links or examples of defconfig for buildroot?

Then, I can share information if those are community contributed.

 

Best regards,

Salas.

0 Kudos
Reply
3,682 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @kanakshilledar 

 

Yes, those repos are external and are not supported by NXP. But it is interesting there are a lot of the NXP devices, maybe I can try one of them and test by my side at the end of the week. 

 

Also, you can try to compile for your desired device and check if those are working or not.

 

Best regards,

Salas.

0 Kudos
Reply
3,661 Views
kanakshilledar
Contributor II

Hello @Manuel_Salas 

These configs are working, but all of them are without GUI, I am looking at ones with GUI.

 

Thanks!

0 Kudos
Reply
3,637 Views
gary_bisson
Senior Contributor III

Hi,

You can use the configuration below meant for Ezurio devices:

https://github.com/boundarydevices/buildroot-external-boundary/blob/master/configs/nitrogen8mm_qt5_g...

It includes weston & qt.

Regards

3,618 Views
kanakshilledar
Contributor II

Hi @gary_bisson 

Thanks for sharing those. I will go through it.

 

Best Regards,

0 Kudos
Reply