GPU hang

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU hang

2,033件の閲覧回数
Salvatore1z
Contributor II

Hello,

I'm running Kernel 3.14.28 on a custom imx6q-based board and I'm having the following problem with the GPU:

[galcore]: GPU[0] hang, automatic recovery.

Once recovery is complete things work. Anyway, recovery causes HMI unavailability...

I have two questions:

1. What is going on with the GPU to have a GPU hang?

2. Is there some recent change/patch which addresses this problem?

Thank you.

Salvatore

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,613件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

You may try the recent BSP L3.14.52, where GPU driver is  upgraded to Vivante v5.0.11p7.4.

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS

Summary Page :

i.MX 6 Series Software and Development Tool|NXP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信