GPP,PPP not accessible

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPP,PPP not accessible

1,744 Views
prathameshghane
Contributor II

Hi developers,

I am trying to build image for Freescale SABRE-AI board using LTIB.

I am working from behind corporate proxy.

According to the documentation, i have done following changes to the ~/.ltibrc file

%http_proxy

http://<usr>:<password>@<proxyserver.com>:8080

My ppp_url and gpp_url are as follows:

%ppp_url

http://auslxsc01.am.freescale.net/ppp/

%gpp_url

http://bitshrine.org/gpp/

(BOTH OF THESE LINKS ARE NOT OPENING THROUGH BROWSER).

I have also set  %ppp_proxy,%gpp_proxy, %gpp_stage_proxy,%cpp_stage_proxy to 1.

When LTIB tries to access some of the packages from gpp, i get the following error.

Processing: libmad

====================

Build path taken because: no prebuilt rpm,

Testing network connectivity

Testing proxy connection for PPP : FAIL

response was: 500 Can't connect to <username>:<password>:80

Can't get ppp index, proxy forced off

Testing proxy connection for GPP : FAIL

response was: 500 Can't connect to  <username>:<password>:80

Can't get gpp index, proxy forced off

No network download connection available

My internet works fine, since I can download other things using curl,wget,sudo apt-get etc.

Plz assist me with this.

Thanks and regards,

Prathamesh Ghanekar

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,404 Views
Raybiztech
Contributor V

Hi prathamesh,

                          I had generated rootfs using ltib successfully. Please find the attachment of .ltibrc i hope it may be helpful.

Thanks & Regards,

Raybiztech.

0 Kudos
Reply