GPIO changes at flashing time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO changes at flashing time

1,555件の閲覧回数
Tanushree
Contributor III

Hello,

We are using imx8dxl processor in our custom board.
We are facing an issue while flashing. The issue one celular module is connected to the processor GPIO. i.e power to the cellular module. if we isolate the GPIO and disconnect the USB from the cellular module then its flashing correctly. How to disable the GPIO in flashing time. During flashing time its starts from initramfs, can we disable in initramfs and how to do that?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,534件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Are you using UUU to program your target board?

0 件の賞賛
返信

1,532件の閲覧回数
Tanushree
Contributor III

Hello @jimmychan 

Yes we are using UUU tool for flashing

0 件の賞賛
返信

1,522件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Do you have the debug console? when UUU is running, you could see the u-boot will up at the console. Then you could stop the u-boot and load another dtb file which is disable the gpio.

0 件の賞賛
返信