GLES2.0 Samples run failed on imx6 linux 3.0.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GLES2.0 Samples run failed on imx6 linux 3.0.35

1,905 Views
forrestjr
Contributor II

imx6 Linux3.0.35(L3.0.35_4.1.0_130816) run i.MX6 Graphics SDK Sample ,the GLES2.0 Samples run failed and GLES1.1 OpenVG run ok.

about failed info :

1、build GLES2.0  samples for FBDEV

2、GLES2.0 Samples run failed log :

       root@freescale /mnt/mmc/GLES20_fbdev$ ./01_SimpleTriangle

      01_SimpleTriangle: SimpleTriangle.c:283: main: Assertion `init()' failed.

       Aborted

      root@freescale /mnt/mmc/GLES20_fbdev$

And debug this error found  glCompileShader() run failed,why?

if use PrecomplieShader(not run glCompileShader()),sample run ok.

L3.0.35_4.1.0_130816 BSP not support GLES2.0?Only support GLES1.1?

Regards,

forrest

Labels (1)
2 Replies

1,613 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi forest,

You can refer to Compile IMX6_GPU_SDK with L3.0.35_1.1.0 and L3.0.35_4.0.0  in our community. Hope it can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,612 Views
forrestjr
Contributor II

Thank a lot,but the problem still exitsts.

Reference "Compile IMX6_GPU_SDK with L3.0.35_1.1.0 and L3.0.35_4.0.0",On imx6 Linux3.0.35(L3.0.35_4.1.0_130816) still only run GLES1.1 and OpenVG Samples.

run GLES2.0 Sample for FBDEV still failed,Eg. run 01_SimpleTriangle

   $./01_SimpleTriangle

   $ glCompileShader error

   $ 01_SimpleTriangle: SimpleTriangle.c:283: main: Assertion `init()' failed.

    $ Aborted

in SimpleTriangle.c

// Compile the shaders

GLuint hVertexShader = glCreateShader( GL_VERTEX_SHADER );

glShaderSource( hVertexShader, 1, &g_strVertexShader, NULL );

glCompileShader( hVertexShader );

// Check for compile success

GLint nCompileResult = 0;

glGetShaderiv( hVertexShader, GL_COMPILE_STATUS, &nCompileResult );

if( 0 == nCompileResult )

{

  char  strLog[1024];

  GLint nLength;

  glGetShaderInfoLog( hVertexShader, 1024, &nLength, strLog );

  printf("glCompileShader error  \n");

  return FALSE;

}

The Shader Compile failed,why? need other config?

0 Kudos
Reply