G2D GPU Cache Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

G2D GPU Cache Questions

2,372件の閲覧回数
jamescovey-crum
Contributor II

We are experiencing AXI bus errors when using the G2D GPU.  This seems to be some race condition as it occurs rarely (it is only seen 1 time out 100 when running our gstreamer application).  Using uncached memory during g2d_alloc() seems to solve the problem, but is not obviously not the best solution.

 

My best theory at the moment is that this is an allocation/deallocation issue occuring whilst the G2D GPU is running.

 

We are using release 5.0.11.p8.6.

 

Specific Questions about g2d (imx-vpu-gpu):

 

1. The g2d_alloc(), g2d_cache_op() functions. Where is the cache? Is this just the ARM caches, or is there some 2d GPU specific cache? My assumption is that this is just managing the ARM caches.

 

2. Is the g2d_cache_op() immediate or is it queued like g2d_copy(), g2d_blit() GPU operations. i.e. do we need to run g2d_finish() to make sure the operation has completed? Obviously if this is just managing the CPU cache then I assume it is immediate.

 

 

This issue is being also progressed on the gstreamer-imx community - 2D GPU AXI BUS error during repeated destruction and creation of pipeline · Issue #172 · Freescale/g... 

 

JamesCC

Original Attachment has been moved to: axi_bus_error.txt.zip

ラベル(5)
0 件の賞賛
返信
1 返信

2,011件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello JamesCC,

I see that the you closed the case and that you posted your findings there (link below)

2D GPU AXI BUS error during repeated destruction and creation of pipeline · Issue #172 · Freescale/g... 

I'm glad the problem looks solved, thank you very much! I'm mentioning this in case it can benefit other users of the Communities.

Regards,

0 件の賞賛
返信