Freescale processor with safety standards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale processor with safety standards

1,522件の閲覧回数
sumeetdube
Contributor III

Hi all,

I wanted to know if any Freescale processor supports following safety and industrial standards

1. Safety level sil4

2. Industry standard IEC61508

3. Automotive standard ISO26262

We would like to use IMX . Does iMX6q support above standards or could it be certified?

Thank you.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,442件の閲覧回数
b36401
NXP Employee
NXP Employee

No. i.MX6q was not certified for these standards.

Sorry for the inconvenience.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------                                                            

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

0 件の賞賛
返信