Framebuffer not detecting image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Framebuffer not detecting image

1,606 Views
abhijeet_ghodga
Contributor III

The command,

fb-test -f 0

generates and displays a test pattern on the screen.

But the command,

cp /home/root/test.jpg /dev/fb0

copies the test image into /dev/fb0 but fails to display anything on the screen.

How to resolve this issue?

Labels (1)
0 Kudos
Reply
1 Reply

1,516 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abhijeet

one can redirect image directly to the framebuffer device as follows:
cat image > /dev/fb0

FSL-UT-FB-003.txt\doc\mxc_fb_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply