Framebuffer issue with Rocko Linux kernels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Framebuffer issue with Rocko Linux kernels

3,040 Views
andrei_faur
Contributor II

Hello,

We are using the i.MX6DP processor on a custom board. Our project was previously based on Yocto Morty but at some point we have decided to migrate to Yocto Rocko. The Linux Kernel version which we used when we ran Morty was 4.1.15. During the migration to Rocko we obviously had to adapt to a newer version of the Linux Kernel.

Our first attempt was to use the 4.9.11 kernel from the meta-freescale repository. We got the following errors:

[    0.518654] ldb 2000000.aips-bus:ldb@020e0008: split mode

[    0.524420] ldb 2000000.aips-bus:ldb@020e0008: split mode or dual mode, ignoring second output

[    0.533710] mxc_sdc_fb fb@0: registered mxc display driver ldb

[    0.574678] imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

[    1.575154] imx-prg 21cd000.prg: wait for buffer ready timeout

[    1.609004] imx-pre 21cb000.pre: timeout waiting for PRE to run out of problematic window for shadow update

[    1.609016] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

[    2.657904] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0

[    3.671258] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0

[    4.177912] mxc_sdc_fb fb@0: timeout when waiting for on the fly config irq

[    4.177917] fbcon_init: detected unhandled fb_set_par error, error code -110

[    6.309572] imx-pre 21cb000.pre: timeout waiting for PRE to run out of problematic window for shadow update

[    6.336961] Console: switching to colour frame buffer device 240x45

[    6.844580] mxc_sdc_fb fb@0: timeout when waiting for flip irq

Later on we have also attempted to use the 4.9.88 kernel from the NXP layers and got the same errors. We have also tried various combinations of layers (like fully using NXP's instead of the community ones), all to no avail, we keep getting the fb errors above.

Some other things worth mentioning:

  • We did not have these issues in 4.1.15 when we were using Morty.
  • We are currently using Rocko with the 4.1.15 kernel. We don't get these issues.
  • We are using framebuffer and eglfs. No X11 and no Wayland.

Has anyone had similar problems? Any ideas on what the issue could be? We would really like to upgrade to a newer kernel version but these errors are preventing us from doing so.

Labels (3)
0 Kudos
Reply
2 Replies

2,555 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Andrei,

 I tried to reproduce without success, everything works and I do not have clue why it fails in newest kernel but the IPU issue happening when you have a splash screen

https://community.nxp.com/thread/455133 

Regards

2,555 Views
andrei_faur
Contributor II

Hello!

Indeed, we are using a splash screen in our project.

I have seen multiple threads refer to these patches:

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

The thread that you linked refers to it as well. We will take a look at the patch and see if it fixes our issue. Do you know why the problem isn't properly fixed in mainline code? Those patches seem to have been getting updates continuously since 2013.

0 Kudos
Reply