Flexcan data transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexcan data transfer

2,302件の閲覧回数
Anushree_Shetty
Contributor I

I am using imx6ull processor, it is taking 2 and half seconds to transfer 384 frames at a bitrate of 500kbps. Is there any way to transfer 384 data frames within a second?

0 件の賞賛
返信
3 返答(返信)

2,293件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anushree

 

> Is there any way to transfer 384 data frames within a second?

 

in general, one can try to increase bitrate x2 or decrease frame size 1/2.

 

Best regards
igor

0 件の賞賛
返信

2,285件の閲覧回数
Anushree_Shetty
Contributor I

Hi igor,

I want to increase the speed for same bitrate and frame size. Is there any option other than increasing the bitrate and decreasing frame size. 

0 件の賞賛
返信

2,274件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anushree

 

in such case you should analyze where delays (if any) between frames happen,
For example remove other running applications, use  MMDC Profiling Tool
0 件の賞賛
返信