FlexSPI DQS STR / SDR query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexSPI DQS STR / SDR query

1,992 Views
DanielNis
Contributor I

According to: https://www.nxp.com/docs/en/data-sheet/IMXRT1160XEC.pdf, 
When defining the FlexSPIn_MCR0[RXCLKSRC] = 0x3,
the FlexSPI controller samples read data on a half delayes DQS falling edge.
DanielNis_0-1690374035958.png
According to JEDEC SFDP for STR / SDR the flash NOR with DQS/DS (data strobe) can work mode (10b):
first rising edge of DS in the middle of the first data bit, start of second data bit aligned with the first falling edge of DS, first rising edge of DS follows a Rising edge of CK.(CLK/SCK)
DanielNis_1-1690374068976.png

Please advised how FlexSPI can also support DQS STR/SDR flash NOR with mode 10b, as described above, as current implementation cause the read to skip first DQS/DS/RWDS clock signal.

Thank you and regards,
Daniel.N



0 Kudos
Reply
3 Replies

1,974 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DanielNis ,

But it seems no problem. There is only a short delay after the clock edge. What is your flash?

 

jingpan_2-1690532547853.png

 

 

 

 

 

Regards,

Jing

 

 

0 Kudos
Reply

1,954 Views
DanielNis
Contributor I

Hi Jing,

Please see the following picture to clearify the issue:

DQS_STR_Isssue_2Aug2023.png

 
Thanks,
Daniel.N

0 Kudos
Reply

1,946 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DanielNis ,

I think RT's datasheet doesn't make it clear. Because actually we don't see such problem.

 

Regards,

Jing

0 Kudos
Reply