FlexCAN single shot mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN single shot mode

2,709件の閲覧回数
madjidlho
Contributor II

Hello,

Single shot mode (also know as one-shot mode) is a transmission mode which will try to send a can frame only once ( no automatic retransmission if there is a transmission error ). For more information about single shot mode you can se SJA1000 manual (http://www.nxp.com/documents/application_note/AN97076.pdf )

We are developing can protocol stacks and in order to implement a time triggered protocol on imx6, we would like to know if single shot feature is available on the can controller.

Thank you for your help.

Best regards,

Madjid

0 件の賞賛
返信
3 返答(返信)

2,445件の閲覧回数
art
NXP Employee
NXP Employee

No, there is no Single Shot Transmission feature implemented in the FlexCAN module of the i.MX6 series processors. Only regular Transmission Abort operation can be performed.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,445件の閲覧回数
madjidlho
Contributor II

Hi Artur, thanks for your fast answer.

Do you know if it is possible to detect arbitration lost with flexCan?

thanks for your feedback.

0 件の賞賛
返信

2,445件の閲覧回数
art
NXP Employee
NXP Employee

The FlexCAN module can detect and signal the transmission error.

Best Regards,

Artur

0 件の賞賛
返信