Dear Team,
I am using i.MX8DXL for my design, below are the queries i am having
a) CPU supports two USB2.0 - In between the two which one i can select for flashing
b) I want USB2.0 for one of Module , can i mux another USB2.0 for flashing & another Module. - like using a USB2.0 2 port HUB - One for flashing other for one module.
Yes I was referring to i.MX8DX
The module should be connected to the hub, OTG as a separate burner
I do not think you can do that:
For the OTG core, there is only one port.
The port can be used as either a downstream or an upstream port.
Do you mean i.MX8DX or could you give us your product part number?